Starting with Proficy CSense
Welcome to Proficy CSense!
Proficy CSense is used to monitor both assets and industrial processes, to pinpoint causes of process variation, and to optimize performance. It is used by process engineers, HMI users, production staff and solution engineers.
Proficy CSense makes use of a suite of components to determine and understand the causes of process deviation in industrial environments. This combination provides the capability for complete and integrated process performance enhancements for a given asset or collection of key performance indicators (KPIs) within an industrial process.
With the release of Proficy CSense 8.5 SP1, we are bundling these components into three editions of the software, each with a unique focus. Each edition is licensed separately. The following is a brief description of each edition, along with the components included in each edition:
-
Troubleshooter Edition, for offline, ad hoc, or on demand process modelling and troubleshooting, which includes the Continuous Troubleshooter and Discrete & Batch Troubleshooter, along with all external connectors, and Action Object Toolkit.
-
Run-time Edition, for the online deployment and monitoring environment, which includes Action Object Services, the Architect, Action Object Toolkit.
-
Developer Edition, for the expert user, trained in analytics and/or with software development experience. This is used for process modelling and troubleshooting, and designing and implementing online monitoring and control solutions. The Developer Edition includes both the Troubleshooter Edition and Run-time Edition components.
Components | Description | Availability |
Continuous Troubleshooter, and Discrete & Batch Troubleshooter |
The Continuous Troubleshooter and Discrete & Batch Troubleshooter enable you to rapidly troubleshoot time continuous, discrete or batch processes by examining production data from a variety of historical data sources. Data is prepared and visualized, and rules-based and data driven process models can be constructed. The knowledge extracted from these models allows you to estimate the benefit of the proposed process changes, all with a few button clicks. Using this modelled system, root causes of process deviations are identified, so processes can be corrected to produce a consistent product at optimal yield levels. |
Troubleshooter and Developer Edition |
Architect |
This comprehensive development platform provides drag-and-drop building blocks to quickly develop scalable, robust solutions. These solutions can then be deployed online, either in real-time or as scheduled events, through the CSense Runtime Manager. A solution is generally developed from a combination of recipes for data preparation, a blueprint of data actions, and a way of sinking data for reuse, either in the CSense Runtime Manager, or a number of third-party applications. |
Run-time and Developer Editions |
Action Object Services |
Action Object Services are used to deploy and execute Action Objects. The actual application used for deployment is the CSense Runtime Manager. The CSense Runtime Manager provides a simple and easy way to deploy and monitor Action Objects. An Action Object (AO) is the name given to an executing configuration, which could have been created and deployed from a number of sources, including Architect and Process+ to name a few. An executing Action Object is an OPC Classic Server and can be connected to from OPC Classic clients. There are different types of Action Objects that can be deployed:
|
Run-time and Developer Editions |
Data Server |
The CSense Data Server is provided with all editions and is a set of databases running on Microsoft SQL Server. These databases are used when doing data preparation from the Troubleshooters, as well for storing Action Objects used by the Action Object Services. |
Troubleshooter, Run-time, and Developer Editions |
Action Object Toolkit |
The Action Object Toolkit is provided with all editions and is geared for advanced users to programmatically create blueprints and Action Objects. This set of software tools also enables the development of deployable Action Objects, created in any number of third-party applications, that can be integrated into the Proficy CSense software. The Action Object Toolkit includes the following sub-components:
|
Troubleshooter, Run-time, and Developer Editions |
MPC Editor |
The MPC (Model Predictive Control) Editor enables engineers to define and configure a model and controller for a Model Predictive Control solution. Once configured, the MPC model and controller can be saved to a file, which is then used to configure the MPC block in the CSense Architect for offline simulation or online real-time execution of the MPC solution. |
Developer Edition |
Refer to your purchase documents for the specific edition you are licensed to use. If any of the required execution files are missing or appear to have been damaged in the distribution process, please contact your Proficy CSense agent or distributor. Alternatively, contact GE Vernova support.
-
Before you begin installing our product, please read this Getting Started Guide. It includes information about the following:
-
Product information
-
Installation requirements and instructions
-
Supported regional settings